SLVAF37 January 2021 ATL431LI
Figure 1-1 is a general current-mode control converter. This type of non-isolated converters integrate the EA (error amplifier) and Vref as parts of feedback control loop. And Type-2 amplifier network provides optimal compensation in the loop.
On the basis of the composition of TL431, Figure 1-2 shows how it can be used as a standard EA.
The pullup resistor (Rbias) value should be chosen to meet the minimum cathode current requirement, this is to provide sufficient bias current to TL431 under all circuit conditions.