SLVAFH1A December 2022 – December 2023 TPS62933 , TPS62933F , TPS62933O , TPS62933P
The output voltage range is the same as when configured as a buck converter, but negative. The output voltage for the inverting buck boost topology should be set between –0.8 V and –22 V. The output voltage is set the same as in the buck configuration, with two resistors connected to the FB pin. Due to the increased noise of the inverting buck boost topology, and for a more robust design, use smaller value resistors than what are used for the buck configuration.