SLVAFP9 October 2024 TPS65219 , TPS6521905
The always ON/cost designed power supply consolidation uses the -1/-2 speed grade devices. This power scheme allows to consolidate the 0.85V domains. When VCCINT and VCCINT_IO/VCCBRAM operate at the same voltage levels, they can be powered by the same supply and ramped simultaneously. If the maximum total current of all the power domains supported by External1 and the PMIC DCDC1 does not exceed 3.5A, all these domains can be supplied by DCDC1. Alternatively, all the 0.85V domains can be supplied by the External1 and the DCDC1 from the PMIC can be re-programmed to supply other power domains in the application.