SLVAFT9 June   2024 TPS61022 , TPS61023

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction of Photovoltaic Cell and MPPT Requirement
  5. 2Typical Battery Powered Outdoor System with PV Panel
  6. 3MPPT Method with Generic DC/DC Converter
    1. 3.1 TPS61023 Introduction
    2. 3.2 Hysteresis Control MPPT Method with TPS61023
    3. 3.3 Experiment Results
  7. 4Summary
  8. 5References

MPPT Method with Generic DC/DC Converter

Some MPPT method regulates the operation voltage of PV panel at MPP accurately, but usual needs a very complex control circuit or algorithm. Considering sometimes the output power of PV panel around MPP is not much worse than the power at MPP, so it is not necessary to take much effort to regulated at MPP accurately. There is a rough but very simple MPPT method called hysteresis control, it means to startup and shutdown the PV system to make sure that the PV panel operates around MPP.

Define VPV_UVLO_rise and VPV_UVLO_fall separately as the startup voltage and shutdown voltage. And the PV system is turned on when the voltage of PV panel is rising to VPV_UVLO_rise (the sunlight becomes stronger), and turned off when the voltage is falling below VPV_UVLO_fall (the sunlight becomes weaker).

Based on this, the engineer needs to program the startup and shutdown voltage of the DC/DC power converter for different types of PV panels.

Figure 3-1 shows a diagram of hysteresis control MPPT method.

 Hysteresis Control MPPT
                    Method Figure 3-1 Hysteresis Control MPPT Method