SLVK174 September 2024 TPS7H1121-SP
The TPS7H1121-SP is packaged in a 22-pin thermally-enhanced ceramic package as shown in Figure 3-1. The TPS7H1121EVM-CVAL evaluation module was used to evaluate the performance and characteristics of the TPS7H1121-SP under heavy ion radiation. The TPS7H1121EVM-CVAL (Evaluation Module) is shown in Figure 3-2. The EVM schematic is shown in Figure 3-3.