SLVSDU6D July 2017 – November 2019
PRODUCTION DATA.
The output current range of the circuit is determined by the equation shown in the configuration. Keep in mind that the VREF equals to 2.5V. When choosing the sense resistor RS, it needs to generate 2.5V for the ATL43xLI when IO reaches the target current. If the overhead voltage of 2.5V is not acceptable, please consider lower voltage reference devices such as TLV43x or TLVH43x.
The output current accuracy is determined by both the accuracy of ATL43xLI chosen, as well as the accuracy of the sense resistor RS. The internal virtual reference voltage of ATL43xLI will be within the range of 2.5 V ±(0.5% or 1.0%) depending on which version is being used. Another consideration for the output current accuracy is the temperature coefficient of the ATL43xLI and RS. Please refer to the electrical characterization table for the specification of these parameters.