SLVSE46A November 2017 – January 2018
PRODUCTION DATA.
The address counter of the pattern sequencer is reset to the value stored in the register on every rising edge of LS_START. At the same time, the signal generator is preset to the values defined in the and registers. Note that the preset registers contain values for master channels only and the same values are applied to master and slave channels.
The first level shifter output may toggle as soon as the seventh rising edge of SEQ_CLK after LS_START is high.