SLVU097B October 2003 – October 2021 TPS54350
The TPS54350EVM-235 is provisioned with a external low-side FET for operation as a synchronous buck regulator. If desired, an external catch diode can be used in place of the FET. The pad for the diode is located on the back side of the PCB. Verify that the inductor is properly sized for operation without the low-side FET. The minimum value for the inductor when operating in this mode is given by Equation 5.