3 Quick Start Guide
The DRV10974 EVM requires a VCC power supply source, which has a recommended operating range from 4.4 V to 18 V. Use the following sequence to power up the EVM:
- Connect the power supply ground to pin 2 (GND) and a voltage between 4.4 V and 18 V to pin 1 of connector P1 (Power In). Set the current limit on the power supply to 1.5 A and make sure switch S1 is in the Off (Up) position as shown in Figure 2.
- Use the default ADV, RMP, and CS resistor values (or set them up in Section 7).
- Determine whether to use an analog voltage or PWM to control the speed of the motor.
- For using an analog voltage to control the speed: match the jumpers as shown in Figure 3 and use the potentiometer (R5) to control the speed.
- For using a PWM signal to control the speed: match the jumpers as shown in Figure 4 and connect the PWM signal to the PWMIN test point.
- Power up the board and turn the switch S1 to the On (Down) position.