SLVUBB4B November 2017 – February 2023
The Filter Designer enables the user to design a differential mode filter, such as the input filter for a power supply. The tool shows the Bode plot of the filter transfer function and the damping circuit and helps with finding a desirable damping circuit (see example in #FIG_CPH_RBC_RVB). In addition, the filter impedance with and without the damping circuit is displayed to determine if the filter is stable or not.