SLVUBT0A June 2020 – January 2021
Terminal J6, labeled VSYS_IN in Figure 2-1 and Figure 2-2, can accept wire gauges up to 14 AWG. The voltage supplied must be within the input range of the device, 2.7 V to 5.5 V. The power supply providing the input to VSYS_IN is required to supply 120% of the output power. Once power has been supplied to VSYS_IN, the pullup on nPWRON/ENABLE pin will enable the device and the power output rails will activate. The default ON Request for the master device is the ENABLE pin which is a level sensitive input. Please refer to SLVSEA7 for more details.