The following sections outline how to configure the TPS65219EVM for general
experimentation.
EVM Configuration
The TPS65219EVM-SKT can be
configured as follows:
- Configure regulator input
supply rails for the expected application using the jumpers indicated in the
"Supply Voltage Setup "
- Configure the multi-function
pins externally using the mode configuration descriptions indicated in
"Multi-Function pin setup". Please note that the default configuration for
regulator choice in SD or DDR voltage selection may differ for each
individual NVM configuration (polarity is configurable).
- Connect VSYS to a power
supply capable of supporting the application and enable the supply. Typical
supply for TPS6521905 is 5V.
- If using a version of
TPS65219 configured for First Supply Detection (FSD), the power-up sequence
is executed as soon as the 5V supply is connected to VSYS.
Note: The TPS6521905 NVM comes with all the power rails disabled by default. When
using this variant, an ON request must be triggered by pressing and releasing
the SW1 push-button so the PMIC can detect a rising edge on the EN/PB/VSENSE pin
and transition to Active state. Once in Active state, the power rails can be
enabled by writing to register ENABLE_CTRL, address 0x02.