2 illustrates the EVM schematic.
Note:
- To evaluate the performance of one
TPS25984 eFuse at lower currents (< 55 A), RZ5, RZ6, RZ7, RZ8, and RZ9 resistors need
to be depopulated. Also R11 and R12 resistors must be populated to disable the secondary
eFuse.
- The ground connections for the various
components around the TPS25984 eFuses must be wired directly to each other and the GND
pins of respective eFuses. This must be followed by connecting them to the system ground
at one point, as implemented using RZ1 and RZ4 resistors in the EVM schematic. Do not
connect the various component grounds through the high current system ground line.