SLVUCH6A July   2023  – November 2023 TPS25984

 

  1.   1
  2.   TPS25984EVM: Evaluation Module for TPS25984 eFuse
  3.   Trademarks
  4. 1Introduction
    1. 1.1 EVM Features
    2. 1.2 EVM Applications
  5. 2Description
  6. 3Schematic
  7. 4General Configurations
    1. 4.1 Physical Access
    2. 4.2 Test Equipment
      1. 4.2.1 Power Supplies
      2. 4.2.2 Meters
      3. 4.2.3 Oscilloscope
      4. 4.2.4 Loads
  8. 5Test Setup and Procedures
    1. 5.1  Hot Plug
    2. 5.2  Start-Up With Enable
    3. 5.3  Difference Between Current Limit and DVDT Based Start-Up Mechanisms
    4. 5.4  Power Up Into Short
    5. 5.5  Overvoltage Lockout
    6. 5.6  Transient Overload Performance
    7. 5.7  Overcurrent Event
    8. 5.8  Provision to Apply Load Transient and Overcurrent Event Using an Onboard Switching Circuit
    9. 5.9  Output Hot Short
    10. 5.10 Quick Output Discharge (QOD)
    11. 5.11 Thermal Performance of TPS25984EVM
  9. 6EVAL Board Assembly Drawings and Layout Guidelines
    1. 6.1 PCB Drawings
  10. 7Bill of Materials (BOM)
  11. 8Revision History

Provision to Apply Load Transient and Overcurrent Event Using an Onboard Switching Circuit

The TPS25984EVM provides an add-on circuit to facilitate load transients and persistent overcurrent events. The implementation consists of three (3) low side MOSFETs (Q4, Q5, and Q6) and a monoshot gate driver circuit (U4 and U5) as well as six (6) onboard load resistors of 1 Ω each (R16 to R21) in parallel. Using a single pole single through (SPST) switch (S1), the monoshot gate driver generates gate signals of 1-ms, 2-ms, 5-ms, 10-ms, and 20-ms durations. By doing this, the low side MOSFETs (Q4, Q5, and Q6) are turned on for that specific duration, creating a load transient in addition to the steady-state load. Use the following instructions to apply a load transient or persistent overcurrent event using this onboard switching circuit:
  1. Configure the Jumper J3 to an appropriate position to obtain required overcurrent blanking period (tTIMER) as per 6.
  2. Configure the Jumper J6 position to desired reference voltage for overcurrent protection and active current sharing as mentioned in 6.
  3. Configure the Jumper J4 in an acceptable position to set required circuit breaker threshold (IOCP) as per 6.
  4. Set the input supply voltage VIN to 12 V and current limit to 200 A.
  5. Connect the power supply between VIN (Connector T1) and PGND (Connector T3), then enable the power supply.
  6. Apply a steady-state load between VOUT (Connector T2) and PGND (Connector T3).
  7. Use the single pole single through (SPST) switch (S1) to configure the transient load turn on duration.
  8. Press the switch SW3 to turn on the Q5, Q6, and Q7 MOSFETs, which creates a load transient of 72 A (typical) between VOUT and PGND with 12-V output.
  9. Observe the waveforms of VOUT (TP6), MOSFET GATE (J9), and input current using an oscilloscope.

Another option is to apply a custom load transient using an external function generator, connected between TP26 and TP27, and the shunt of jumper J9 set to "2-3".

CAUTION:

In that case, make sure to limit the transient load current magnitude to a safe level for reliable operation of the load resistors (R16 to R21) based on their maximum permissible peak pulse power vs pulse duration plot.

Figure 5-15 and Figure 5-16 show the test waveforms of transient overload and persistent overload events respectively using the on-board switching circuit.

GUID-20220922-SS0I-H1SZ-LQ7W-8LK3SLQZJ4P1-low.svg
VIN = 12 V, CITIMER = 22 nF, COUT = 470 μF, RIMON = 1.1 ∥ 1.1 kΩ, RIREF = 40.2 kΩ, IOUT (Steady-State) = 100 A, and IOUT (Transient) = 69 A for 9 ms
Figure 5-15 Transient Overload Performance in TPS25984EVM Using the Onboard Switching Circuit
GUID-20220922-SS0I-TGG1-LMLV-MX4RKCZ2TWBB-low.svg
VIN = 12 V, CITIMER = 22 nF, COUT = 470 μF, RIMON = 1.1 ∥ 1.1 kΩ, RIREF = 40.2 kΩ, IOUT (Steady-State) = 100 A, and IOUT (Transient) = 69 A for 18 ms
Figure 5-16 Persistent Overload Performance in TPS25984EVM Using the Onboard Switching Circuit