Use the following instructions to perform the power up into short test:
- Set the input supply voltage VIN to 12 V and current limit to 100 A. Connect the supply between VIN (Connector T1) and PGND (Connector T3) and keep the power supply OFF.
- Short the output of the EVM. For example, VOUT (Connector T2) to PGND (Connector T3) through a
short and thick cable to make sure the short-circuited path impedance is minimum
as possible.
- Configure the Jumper J6 position to desired reference voltage for overcurrent protection and
active current sharing as mentioned in 6.
- Configure the jumpers J5 and J7 positions to the desired current limits during start-up as
mentioned in 6.
- Keep the TPS25984 eFuses disabled by pushing the switch SW1.
- Turn ON the power supply.
- Enable the TPS25984 eFuse by releasing the switch SW1.
Figure 5-8 and Figure 5-9 show the test waveforms of power up into output short on the
TPS25984EVM eFuse Evaluation Board with two (2) devices in parallel.
Note: During power up into short, a thermal fold-back
results in the current flowing through the device being less than the calculated
value of the current limit during start-up.
VIN = 12 V, EN
stepped up from 0 V to 3 V, RILIM = 402 Ω, RILIM2 =
402 Ω, RIREF = 40.2 kΩ, CITIMER = 22 nF, and OUT
shorted to PGND
Figure 5-8 Power Up Into Output Short Response of
TPS25984 eFuseVIN = 12 V, EN
stepped up from 0 V to 3 V, RILIM2 = 402 Ω, RIREF =
40.2 kΩ, RIREF = 40.2 kΩ, CITIMER = 22 nF, and OUT
shorted to PGND
Figure 5-9 Power Up Into Output Short Response in
TPS25984EVM: Current Sharing Between Two (2) eFuses