Use the following instructions to perform the output hot short test:
- Set the input supply voltage VIN to 12 V and connect the power supply between VIN (Connector T1) and PGND (Connector T3).
- Turn ON the power supply.
- Short the output of the device for example, VOUT (Connector T2) to PGND
(Connector T3) through a shorter cable, which is just enough to insert a 150 A
current probe.
- Observe the waveforms using an oscilloscope.
Figure 5-17 shows the test waveforms of output hot short on the TPS25984EVM with two (2)
TPS25984 eFuses in parallel.
Important: Make sure there is sufficient input capacitor to eliminate voltage dips at the input. A combination of electrolytic and ceramic capacitors are preferred. With these capacitors, a large current can be provided for a short period of time during short-circuit.
Note: Obtaining repeatable and similar short-circuit
testing results is very difficult. The following contributes to the variation in
results:
- Source bypassing
- Input leads
- Board layout
- Component selection
- Output shorting method
- Relative location of the short
- Instrumentation
The actual short exhibits a certain degree of randomness because the short
microscopically bounces and arcs. Make sure that configuration and methods are used
to obtain realistic results. Hence, do not expect to see waveforms exactly like the
waveforms in this user's guide because every setup is different.