Use the following instructions to perform
the start-up with current limit test:
- Configure the jumper J2 position to the desired slew rate mentioned in 6.
- Configure the jumpers J5 and J7 positions to the desired current limits during start-up
as mentioned in 6.
- Configure the Jumper J6 position to desired reference voltage for overcurrent protection
and active current sharing as mentioned in 6.
- Set the input supply voltage VIN to 12 V and current limit to 100 A.
- Connect a load of 0.9 Ω between VOUT (Connector T2) and PGND (Connector T3).
- Connect the input supply between VIN (Connector T1) and PGND (Connector T3).
- Turn on the power supply by keeping the device disabled using the switch SW1.
- Enable the eFuse by releasing the switch SW1.
- Observe the waveform at VOUT (TP6) and input current using an oscilloscope. The main
intention of this experiment is to observe the output voltage and input current profiles
and time required to complete the inrush with two different ILIM set points having all
other test conditions identical. The inrush current hits the current limit set point in
one case, but does not in the next.
Figure 5-6 and Figure 5-7 show the difference between the current limit and DVDT based start-up mechanisms on the
TPS25984EVM eFuse evaluation board having two (2) devices in parallel for RILIM
of 680, RLIM2 of 680 Ω, RILIM of 402, and RLIM2 of 402
Ω.
VIN =
12 V, EN stepped up from 0 V to 3 V, RILIM = 680 Ω, RLIMI2 = 680
Ω, RIREF = 40.2 kΩ, COUT = 18.47 mF, RLOAD = 0.9 Ω, and
CDVDT = 33 nF
Figure 5-6 Start-Up With Current Limit Response
of TPS25984 eFuseVIN =
12 V, EN stepped up from 0 V to 3 V, RILIM = 402 Ω, RILIM2 = 402
Ω, RIREF = 40.2 kΩ, COUT = 18.47 mF, RLOAD = 0.9 Ω, and
CDVDT = 33 nF
Figure 5-7 Start-Up With Output Slew Rate
Control (Only) Response of TPS25984 eFuse