SLVUCH7A september   2022  – june 2023 TPS25990

 

  1.   1
  2.   TPS25990EVM: Evaluation Module for TPS25990 eFuse
  3.   Trademarks
  4. 1Introduction
    1. 1.1 EVM Features
    2. 1.2 EVM Applications
  5. 2Description
  6. 3Schematic
  7. 4General Configurations
    1. 4.1 Physical Access
    2. 4.2 Test Equipment and Setup
      1. 4.2.1 Power supplies
      2. 4.2.2 Meters
      3. 4.2.3 Oscilloscope
      4. 4.2.4 USB-to-GPIO Interface Adapter
      5. 4.2.5 Loads
  8. 5Test Setup and Procedures
    1. 5.1  Hot Plug
    2. 5.2  Start-up with Enable
    3. 5.3  Current Limit Based Start-up Behavior
    4. 5.4  Power Up into Short
    5. 5.5  Overvoltage Lockout
    6. 5.6  Transient Overload Performance
    7. 5.7  Overcurrent Event
    8. 5.8  Provision to Apply Load Transient and Overcurrent Event Using an Onboard Switching Circuit
    9. 5.9  Output Hot Short
    10. 5.10 Quick Output Discharge (QOD)
    11. 5.11 Thermal Performance of TPS25990EVM
  9. 6Using the TPS25990EVM-GUI
    1. 6.1 Access the TPS25990EVM-GUI
    2. 6.2 Introduction to the TPS25990EVM-GUI
    3. 6.3 Establishing Communication Between the EVM and GUI
    4. 6.4 Quick Info
    5. 6.5 Configuration
    6. 6.6 Telemetry
    7. 6.7 Blackbox
    8. 6.8 Register Map Page
  10. 7EVAL Board Assembly Drawings and Layout Guidelines
    1. 7.1 PCB Drawings
  11. 8Bill Of Materials (BOM)
  12. 9Revision History

Telemetry

The Telemetry page as shown in Figure 6-10 guides the user through the device parametric data, status information, data read from the high speed sample buffer, and real time graphical plots of a few key device parameters.

GUID-20230525-SS0I-KS2D-FMZG-BMPZB72JQVGM-low.svg Figure 6-10 TPS25990EVM-GUI: Device Telemetry

This portion of the GUI is divided into five tabs, Telemetry Configuration, Device Parametric Information, Device Status Information, Read High Speed Sample Buffer, and Parametric Plot.

Telemetry Configuration tab includes the following registers as shown in Figure 6-11:

  • ADC_CONFIG_1 (E8h)
  • Bit[7] of ADC_CONFIG_2 (E9h)
  • PK_MIN_AVG (EAh)
GUID-20230525-SS0I-RF1H-8DG0-Q2HPNXWTTVH3-low.svg Figure 6-11 TPS25990EVM-GUI: Device Telemetry: Telemetry Configuration

Accessibility of the ADC_CONFIG_1 (E8h) register is disabled in the GUI. Changing the configuration of this register is not recommended under normal operation. This is because changing the configuration of this register prevents the ADC from sampling all the necessary signals needed for protection.

Device Parametric Information tab contains the following registers as shown in Figure 6-12 to represent real world values of all the parameters reported by the device:

  • READ_VIN (88h)
  • READ_VOUT (8Bh)
  • READ_IIN (89h)
  • READ_TEMPERATURE_1 (8Dh)
  • READ_PIN (97h)
  • READ_VAUX (D0h)
  • READ_VIN_AVG (DCh)
  • READ_VIN_MIN (D1h)
  • READ_VIN_PEAK (D2h)
  • READ_VOUT_AVG (DDh)
  • READ_VOUT_MIN (DAh)
  • READ_IIN_AVG (DEh)
  • READ_IIN_PEAK (D4h)
  • READ_TEMP_AVG or READ_VAUX_AVG (D6h)
  • READ_TEMP_PEAK (D7h)
  • READ_PIN_AVG (DFh)
  • READ_PIN_PEAK (D5h)
  • READ_EIN (86h)
GUID-20230525-SS0I-CTK7-9DPR-S0HQZ2JDTFSR-low.svg Figure 6-12 TPS25990EVM-GUI: Device Telemetry: Device Parametric Information: General Parameters

The GUI implements the algorithm described in the PMBus Specifications for computing the real-world value of accumulated energy and average power consumption by the system using READ_EIN (86h) register data as presented in Figure 6-13. To get the values of accumulated energy and average power consumption, the READ_EIN (86h) register must be read periodically with a periodicity specified in the Energy Refresh Rate field and by enabling the Read Energy toggle switch as indicated by the RED circle in Figure 6-13. ADC HI PERF toggle switch (Bit[3] of DEVICE_CONFIG (E4h) register) specifies the ADC internal operating modes, high speed or high performance. The effective ADC sampling period is 11 µs in high speed mode and 18 µs in high performance mode and comes with high speed mode by default. If changing the ADC internal modes is necessary, then changing the ADC internal modes must be done before the load is applied and after establishing communication with the GUI for the first time. Changing the ADC internal modes must not be changed under normal operation. This results in the wrong real world value for energy accumulation.

GUID-20230525-SS0I-MMDS-DX7J-RPXL4TGP1MPR-low.svg Figure 6-13 TPS25990EVM-GUI: Device Telemetry: Device Parametric Information: Energy Parameters

Device Status Information tab contains the following registers as shown in Figure 6-14 to represent the device status:

  • STATUS_INPUT (7Ch)
  • STATUS_WORD (79h)
  • STATUS_OUT (7Ah)
  • STATUS_TEMP (7Dh)
  • STATUS_CML (7Eh)
  • STATUS_MFR_SPECIFIC (80h)
  • STATUS_MFR_SPECIFIC_2 (F3h)
  • BB_TIMER (FAh)
GUID-20230525-SS0I-L09D-RFZ6-CQJN2R8DT0WK-low.svg Figure 6-14 TPS25990EVM-GUI: Device Telemetry: Device Status Information

Device parametric and status information can be updated manually or automatically as selected in the Update Mode drop-down menu shown in Figure 6-15. In manual update mode, users need to click on the UPDATE STATUS icon to get the latest information. Upon clicking the START icon in automatic update mode, the GUI reads all telemetry registers except READ_EIN (86h) in a time interval specified in the Update Rate field, as shown by the RED circle in Figure 6-15. The GUI continues to read the registers as long as the user is in any one of the three tabs, Telemetry Configuration, Device Parametric Information, and Device Status Information under the Telemetry page. The GUI stops updating as the user navigates to other tabs.

GUID-20230525-SS0I-C5Z8-HDCN-DFBDVXP9K9BK-low.svg Figure 6-15 TPS25990EVM-GUI: Device Telemetry Update

Read High Speed Sample Buffer tab implements the READ_SAMPLE_BUF (D8h, Block Read) register. The ADC channel to sample for buffering and the decimation rate/sample skip count are configured through Bit[5:3] and Bit[2:0] respectively in the ADC_CONFIG_2 register. Parameter selection and decimation rate can be picked using the drop-down menus as shown by the RED circle in Figure 6-16. By selecting different decimation rates, users can choose between fine time resolution & short aperture and coarse time resolution & wide aperture. Click on the READ icon to plot the 64 samples retrieved from the READ_SAMPLE_BUF block read command as shown in Figure 6-16.

GUID-20230529-SS0I-8FCB-S4CW-BGNSB19R5VVC-low.svg Figure 6-16 TPS25990EVM-GUI: Device Telemetry: Read High Speed Sample Buffer: Input Current

Figure 6-17 represents the plots of input and output voltages (during a load transient event) using the data retrieved by sending the READ_SAMPLE_BUF (D8h) block read command at two different times.

GUID-20230529-SS0I-NW5P-9F2D-JJVKP12K3WQ6-low.svg Figure 6-17 TPS25990EVM-GUI: Device Telemetry: Read High Speed Sample Buffer: Input and Output Voltages

Parametric Plot tab allows users to visualize some key device parameters, including input voltage, output voltage, input current, input power, average input power, device die temperature, auxiliary input voltage, and energy accumulation as shown in Figure 6-18. Users must select the update rate from the drop-down menu called Update Rate as presented by the RED circle in Figure 6-18. Then, users need to choose the parameters to plot. To begin plotting, two parameters must always be selected. Click on the START icon to initiate plotting. Plotting can be stopped by clicking on the STOP icon. Plotting stops as the user navigates to other tabs. Figure 6-19 shows a sample plot window with input power and energy accumulation.

GUID-20230529-SS0I-D0VF-GCV6-W91TZKPQ2BPW-low.svg Figure 6-18 TPS25990EVM-GUI: Device Telemetry: Parametric Plot
GUID-20230529-SS0I-MJL3-CW5T-GH4ZNNMZGDVB-low.svg Figure 6-19 TPS25990EVM-GUI: Device Telemetry: Parametric Plot: Input Power and Energy Accumulation