The following procedure outlines the steps to be taken for using the TPSM365R15EVM and TPSM365R15FEVM. Use this section in conjunction with Section 3 to correctly setup the EVM.
- Determine the output voltage that is to be evaluated, then reference Section 2. This table provides the recommended jumper configurations.
- After making any required changes, confirm that the output voltage is within a couple percent of the set output voltage.
- Verify the performance of the EVM and compare with applicable curves within this user's guide.
- Consult on e2e if there are concerns in the evaluation of this device.
Table 2-1 Suggested Frequency and Output Voltage SettingsVOUT (V) | Suggested Frequency |
---|
1.8 | 500 kHz |
2.5 | 500 kHz |
3.3 | 1 MHz |
5 | 2.2 MHz |
12 | 2.2 MHz |