SLVUCO7 March   2023 TPSM83100

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
    1. 1.1 Background
    2. 1.2 Performance Specification
    3. 1.3 Modifications
      1. 1.3.1 IC U1 Operation
      2. 1.3.2 Device Evaluation
  4. 2Setup
    1. 2.1 Input/Output Connector and Header Descriptions
    2. 2.2 Setup
    3. 2.3 Precautions
  5. 3Board Layout
    1. 3.1 Layout
  6. 4Schematic and Bill of Materials
    1. 4.1 Schematic
  7. 5Bill of Materials

Input/Output Connector and Header Descriptions

    J1, Pin 1 and 2 – VINPositive input connection from the input supply for the EVM
    J1, Pin 3 and 4 – S+/S– InputVoltage sense connections. Measure the input voltage at this point.
    J1, Pin 5 and 6 – GNDVIN GND return connection from the input supply for the EVM, common with J2, pin 5 and 6
    J2, Pin 1 and 2 – VOUTOutput voltage connection
    J2, Pin 3 and 4 – S+/S– VOUTOutput voltage connection
    J2, Pin 5 and 6 – GNDVOUT GND return connection for the output voltage, common with J1 pin 5 and 6
    JP1 – EnableShorting the jumper between the center pin EN and HIGH turns on the unit. Shorting the jumper between the center EN and LOW turns the unit off.
    JP2 – MODEShorting the jumper between the center pin MODE and LOW enables automatic transition to power-saving mode at light-load currents as described in the data sheet. Shorting the jumper between the center pin MODE and HIGH enables forced PWM mode.