SLVUCS3 October 2023
The Texas Instruments TPS274C65CPEVM is an evaluation module that is used to demonstrate and showcase all of the features of the underlying TPS274C65 industrial high side switch. This evaluation board provides a seamless way to connect a set of power supplies to the inputs of the TPS274C65, connect loads to the output channels, and switch on and off the device using the control pins of the chip itself, and easily assert and deassert logic signals by the use of a set of external hardware jumpers.. An on-board 3.3-V buck-converter is included on the EVM to allow for external VDD.