SLYU064A June 2023 – December 2023 TMAG3001 , TMAG5170 , TMAG5170-Q1 , TMAG5170D-Q1 , TMAG5173-Q1 , TMAG5253 , TMAG5273
The magnetic implementation corresponds to the type of magnet, the path of motion, and the orientation of the magnet and sensor relative to each other. Figure 2-2 shows a couple possible magnetic implementations per mechanical method introduced in Figure 2-1. Starting from the left, there are two mechanical method 1 options with either a sphere or cylindrical magnet. Then in the middle are two mechanical method 2 options with either a axial ring magnet or a diametric ring magnet. Lastly on the right are two mechanical method 3 options, with one having a central axial ring magnet on the joystick shaft, while the other has two bar magnets that rotate with the axles. Each of these has unique design challenges and may have a unique sensor pairing.