Getting the most out of a RF signal chain design partly depends on providing a low phase noise, clean clock to the A/D converter. In this application report, phase noise data taken using the Texas Instruments’ LMX1204 clock distribution device is studied. In general, the phase noise performance of any clock distribution method, is not only dependent upon the phase noise of the input clock source, but also the active clock signal chain as well. In this case the LMX1204 will be studied in both single and cascaded configurations. In general, the performance measurements confirm the operational ability of the LMX1204 device to provide as an adequate distribution method, up to 16 channels, with minimal degradation in converter performance.
All trademarks are the property of their respective owners.
When numerous devices in a system require a shared clock source, distributing the clock signal inadequately leads to degradation in system performance. This becomes a prevalent concern for applications utilizing digital beamforming (phased array radar, communications, ultrasound) as signal distortion increases directly as a result of increased clock jitter. The LMX1204 is a clock distribution device designed for applications requiring minimal added phase noise within the frequency range 300 MHz to 12.8 GHz. Although the LMX1204 is a high-speed clock distribution device allowing for buffered, multiplied, and divided output frequency (relative to the input frequency), this report will focus solely on the performance of this device in a buffered (1-to-1) configuration.
The LMX1204 creates up to four copies of an input signal, including the ability to buffer, multiply, or divide the signal to each of the outputs. This device distributes a single low power clock signal and with minimal added phase noise per stage. This design supports a two-level cascaded implementation creating 16 output clocks for distribution as shown in Figure 1-1.
The purpose of this design is to show that the signal degradation caused by cascading two LMX1204 devices is minimal. If a design requires cascading multiple LMX1204 devices, we can expect the signal integrity to be very good, as shown in Results.
One aspect taken into consideration for this design was the board size, which was heavily determined by the number of inputs and outputs this design requires. As shown in Figure 1-2, the design uses the Samtec Bull's Eye Connector to ease the board size constraint created by 40 output differential pairs. All 20 outputs of a single LMX1204 device pass through a connector that takes up only 630mm2, less than 1/4 of the equivalent PCB footprint using typical edge mounted SMA connectors.