All trademarks are the property of their respective owners.
The LMK04832-SP, 5962R1723701VXC(1), uses the BiCMOS8B+ process which has been shown not to exhibit Enhanced Low Dose Rate Sensitivity (ELDRS)(2). Per MIL-STD-883 Test Method 1019(3), if an analog product is on a process that has been shown to be ELDRS-free, Total Ionizing Dose (TID) Radiation Lot Acceptance Testing (RLAT) may be done at high dose rate (HDR). In the case of BiCMOS8B+, HDR testing is the worst case condition and covers low dose rate (LDR) applications.
For RLAT of a single wafer, the sample size is 2 units for products with over 4,000 transistors per MIL-PRF-38535(4).
When tested at HDR, it is possible that one parameter might drift outside the electrical test limit at 100 krad(Si). Per TM1019, if this occurs, the units that have readings outside a test limit are put on a room temperature anneal (RTA). If after the RTA all tests recover and all readings are within the test limits, the lot is qualified for 100 krad but only for lower dose rates. The maximum dose rate is calculated by dividing the TID rating by how long the DUT was on RTA before it recovered. For more details and validation of the RTA test method on TI processes, see SNAA156.
The devices under test (DUTs) were put through a 240-hour burn-in with the units biased and operational at 125°C ambient prior to the radiation testing.
Irradiation and electrical testing were done at Texas Instruments Radiation Test Facility in Santa Clara, California.
The DUTs were placed in socketed bias boards, powered up and programmed using Texas Instruments USB2ANY module and TICS Pro software prior to irradiation(5). The supply voltage was set to 3.4 V as measured on the DUT boards. The DUTs were configured so that the PLL2 loop was active and the signal to the Divider and Delay blocks was at 3.2 GHz. Different delays and frequency dividers were used on the different outputs to exercise the different components of the control circuits. The outputs were configured so that at all of the output configurations options, CML, LVPECL, LCPECL, HSDS, LVDS, and 2xLVCMOS were exercised on at least one output each.
DUT #3 went through 48-hour RTA with the DUT in the bias board and powered and configured to the same conditions as during the irradiation.
The DUTs were electrically tested at 0, 50 and 100 krad(Si) and DUT #3 was tested after the 48-hour RTA. All specified data sheet and SMD parameters were tested. In addition to the specified parameters, the test program tests many other parameters to ensure the proper operation of the device. Limits are set using a six sigma baseline. Tests are performed with the supply voltage at 3.135, 3.3 and 3.465 V. There are over 7000 parameters tested.
Wafer lot | V009FOGX |
Wafer number | 21 |
DUT serial numbers | 3, 4 |
Test Location | Texas Instruments, Santa Clara, CA |
Bias board schematic | 291CR17 |
Bias board edge number | 6609056A |
Supply voltage | 3.4 V |
Supply current | 570 mA |
TICS Pro program | Single Loop-CLKin1=1MHz-8_Outputs_VCO1=3200MHz_rev2.txt |
VCO and PLL frequency | 3.2 GHz |
Test programs | GCR4832HB, GQR4832HB |
Electrical test supply voltage | 3.135 V, 3.3 V, 3.465 V |
Dose Rate | 61.5 rad(Si)/s |
Test points | 0, 50, 100 krad(Si) |
RTA | 48 hours |
Test dates | October 28 and 30, 2020 |