The LMK04832EVM-CVAL evaluation module (EVM) provides a platform to evaluate the performance and features of the LMK04832-SP Space Grade Ultra-Low-Noise JESD204B Dual-Loop Clock Jitter Cleaner from Texas Instruments. The user’s guide describes how to set up and operate the EVM. The LMK04832-SP device on each EVM is an Engineering Model, intended for engineering evaluation only. The devices and EVMs are not suitable for qualification, production, radiation testing or flight use.
PLLatinum is a registered trademark of Texas Instruments.
All other trademarks are the property of their respective owners.
Table 1 lists the components found in the evaluation board kit.
HSDC005 | |
---|---|
Evaluation Board | (1) LMK04832EVM-CVAL Evaluation Board with VCXO |
Communication Interface | (1) USB2ANY |