SNAU260A October 2020 – February 2021 LMK5C33216
ADVANCE INFORMATION
The outputs page shows all the possible source frequencies to the output channels. To simplify settings fields necessary to providing an output frequency, a source mux lists all possible sources for each output. Be sure to enable/disable desired outputs at right hand side.
There are many detailed output pages beneath the Outputs page illustrated below showing individual controls for each set of outputs.
The black line between OUT2 to OUT3, OUT4 to OUT7,OUT8 to OUT13, and OUT14 to OUT15 signifies that all these outputs should source from the same VCO.