After the 3.3-V power supply has been
connected and power has been applied to the EVM, connect the USB cable from the PC to
the EVM. The USB interface will provide the necessary power to enable the onboard
USB2ANY controller. A firmware update may be required; if prompted, see
Appendix B for more details.
Run TICS Pro software and open the
device profile:
- From the top-menu, click
Select Device → Clock Distribution with Divider → LMX1204
- The device's Main Page
will load. The default profile is configured for 800-MHz buffer mode.
- From the top-menu, click USB
communications → Interface. Ensure that the selected interface is
USB2ANY and that the correct controller is selected. To confirm
controller selection, click the Identify button to blink the onboard
green communications LED several times in rapid succession; the LED will return
to solid green when complete. After confirming the USB2ANY connection, close the
interface window.
- Ensure that the main window now shows the USB2ANY connection
over SPI.