SNAU273 December   2022 LMX2820

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2SYNC Category
  5. 3SYNC Examples
    1. 3.1 Category 1 SYNC Example
    2. 3.2 Category 2 SYNC Example
    3. 3.3 Category 3 SYNC Example
  6. 4Other Considerations When Using SYNC
  7. 5References

Category 1 SYNC Example

The following is a Category 1 SYNC configuration, because:

  • M = 1 (Doubler and MULT are not used)
  • fOUT is an integer multiple of fOSCIN (6000 / 100 = 60)
  • Channel divider is bypassed (output frequency = VCO frequency)

Figure 3-3 Category 1 SYNC Configuration

With this configuration, the outputs are in phase after programming the LMX2820 devices. The output phases remain constant if:

  • LMX2820 is powered down and powered up again
  • VCO is calibrated again
  • LMX2820 is reset and re-programmed

GUID-20221114-SS0I-8WBJ-4PBX-WQZMHCNWG6BP-low.pngFigure 3-4 Category 1 SYNC Result

Below is another Category 1 SYNC configuration example. This configuration has enabled the Doubler:

  • M = 2 (Doubler is enabled)
  • Channel divider is bypassed
  • fOUT is an integer multiple of M × fOSCIN (6000 / 200 = 30)
  • PLL_NUM = 0

Figure 3-5 Category 1 SYNC With Doubler

If only one of the LMX2820 devices has the Doubler enabled, although both configurations are Category 1 SYNC, the Doubler introduces addition delay in the input path. This delay is carried forward to the output. As a consequence, the phases of the LMX2820 outputs are not exactly in phase. To get exact phase match between multiple LMX2820 devices, the configurations should be identical.

GUID-20221031-SS0I-FGVC-G3FF-7SBDXXCDDQZZ-low.pngFigure 3-6 Phase Offset Due to Unsymmetrical Configuration