There are several settings which must be correct to achieve SYSREF outputs.
- Make sure of the following settings:
- Set SYSREF_MODE to
Continuous (for debugging).
- SRREQ_MODE field set
to SYSREFREQ mode.
- SRREQ_VCM set for
DC-coupled, with about 1.1 V on SYSREFREQ_P and 1.5 V on
SYSREFREQ_N.
- SYSREF_DLY_BYP field
set to use delay.
- SYSREF_EN=1.
- Make sure the frequencies of the SYSREF_DLY_DIV,
SYSREF_DIV_PRE, and SYSREF_DLY_ADJ are correctly configured. The GUI
highlights any frequency violations.
- Make sure that FINTERPOLATOR %
FSYSREF = 0. The GUI highlights the SYSREF divider in case of
violations.
- Make sure that the output channel
(CHx_EN/LOGIC_EN) and the SYSREF buffer (SYSOUTx_EN / LOGISYS_EN) are
enabled.
- Confirm that Windowing mode is not enabled on the User Controls page (SYSWND_EN=0).
- Confirm that R15[9]=1. This is set automatically
by the GUI, so this potential root cause is rare.
- Confirm the 1.1-V and 1.5-V source for
SYSREFREQ_N and SYSREFREQ_P respectively are actually resulting in the
required voltages at the pins. If power supplies are used for these
voltages, then for the supplies to be unable to sink current is uncommon.
The 1.1-V source is not able to sink current from the 1.5-V supply through
the internal 100-Ω impedance. An arbitrary function generator is recommended
if possible.