The on-board USB2ANY interface provides a bridge
between TICS Pro software and the LMX1205 device. When the on-board USB2ANY
controller is first connected to a PC, or if the firmware revision for the
controller does not match with the version used by TICS Pro, a firmware update to
the controller is required.
- Connect the USB cable from the PC to the EVM. The USB interface provides the
necessary power to enable the on-board USB2ANY controller.
- After Windows has set up a USB device, run TICS Pro in the PC.
- The next screen looks like the
image below.
- Click OK, then the screen
looks like the image below. Click Update Firmware.
- Then the
screen below appears.
- Click the Close button to close the window.
- A TICS Pro default device pops
up. Check to make sure that we get a green light on Connection Mode at the
bottom of the GUI.
- Go to the menu bar, click USB
Communications, then select Interface.
- Click
the Identify button, the LED in the USB2ANY interface flashes.
- Now, the USB2ANY is ready to use. Click the Close button to close the
window.