If not already installed, then
install TICS Pro software from TI website: TICS Pro
Software GUI.
Start TICS Pro software.
Select the LMKDB1204 profile from
Select Device → Clock Distribution with Divider →
LMKDB1204.
Confirm communication with the board:
Click USB
Communication from the menu bar.
Click Interface to
launch the Communication Setup pop-up window.
Confirm the following
fields from the Communication Setup pop-up window:
Make sure
USB2ANY is selected as the interface.
In case of
multiple USB2ANY, select desired interface. If a USB2ANY is
currently in use in another TICS Pro, then the user must release
that interface by changing the interface setting to
DemoMode.
Click
Identify to blink LED shown in Figure 3-1. After clicking the Identify button, the LED flashes
quickly at about 0.5 second on, 0.5 second off for about 5
seconds. This confirms the connection to the board. However, be
aware that USB2ANY devices that are connected to the PC, but not
attached to a TICS Pro profile, can blink at a slow rate of 1
second on, 1 second off continuously.
Confirm all the fields
match the ones shown in Figure 3-2.