SNIU051 March 2023
The TMP4718EVM includes several LEDs which indicate the status of the board at any time. The green LED D2 illuminates when power is supplied to the VDD net. The VDD net is connected directly to pin 1 of the TMP4718. The red LED D6 is a status LED for the MSP430F5526. #GUID-B11DAF7E-162A-4144-8FD9-A48C4FF1978C/GUID-87ED5CD9-6E9B-420C-BB46-FB421603C5AC summarizes the functions of D6.
D6 LED STATUS | MEANING |
---|---|
Off |
USB2ANY controller is unpowered or still initializing |
Blinking |
USB2ANY controller is powered but not connected |
On |
USB2ANY controller is connected |
The ALERT and T_CRIT LEDs illuminate when the corresponding ALERT and T_CRIT device pins are asserted. The default value of the Remote and Local T_CRIT limits are adjustable with the use of the ALERT and T_CRIT pullup resistance values. The TMP4718EVM has 10.5-kΩ pullup resistors on ALERT and T_CRIT, which sets 0x65 (101°C) as the default value of registers 0x19 and 0x20. Refer to the TMP4718 data sheet for more information on the adjustable T_CRIT limit.