SNLA224A June 2014 – January 2024 DS90UB913A-Q1 , DS90UB954-Q1 , DS90UB960-Q1
VPoC noise is the measurement of noise introduced into the system from serializer and sensor operation. Figure 4-2 shows a typical waveform measured from the input of the DC regulators. The supply noise is introduced from the switching of DC buck regulators, and the pulse is due to the switching of the sensor. During periods of blanking, the current draw from the sensor is significantly lower than during active periods, which causes the voltage to spike.
The VPoC must meet the following requirements for proper FPD-Link operation.
The VPoC of a PoC network can be measured with the following procedure.