SNLA356 September 2020 DS90UB941AS-Q1 , DS90UH941AS-Q1
When DS90UB941AS-Q1 is operated in DSI Reference Clock Mode, the DSI clock from the source is used to directly set the FPD-Link forward channel frequency and video PCLK rate. It is important to ensure that the DSI clock is continuous (no LP-11 transitions) at all times. For continuous clock mode, the clock lane remains in high-speed mode with a constant frequency at all times. For non-continuous clock mode, the clock lane may enter the LP-11 low power state between HS data packet transmissions.
Symptoms:
How to Verify:
To verify that the DSI clock is continuous, the system designer can probe the DSI clock lane during video transmission. This can be done with a single ended probe attached between one of the data lane P/N nets and GND. The goal is to set the oscilloscope trigger to capture the LPTX amplitude only, while ignoring the HS data transmission.
During HS mode transmission, the clock is expected to have a common mode voltage between 150 mV-250 mV and a differential swing of 140 mV-270 mV.
During Low Power Mode (LP-11), the P/N clock lanes will no longer be differential. They will both transition to the LPTX high level output voltage of 0.95 V-1.3 V.
Set the oscilloscope trigger level to 800mV and monitor the clock lane activity. If the scope does not trigger from the 800mV level, then the DSI clock is continuous. The clock should show continuous toggling activity with a differential swing of ~140 mV - 27 0 mV and a common mode of ~150 mV-250 mV
Resolution:
The DSI source must be configured to enable DSI continuous clock mode. Consult the kernel driver manual for the DSI source for options to enable this behavior which is sometimes referred to a "High Power Mode". Some examples of flags in the DSI source driver pertaining to this configuration are: