SNLA417 January 2023 DP83TC812R-Q1 , DP83TC812S-Q1
Table 4-1 shows the timeline for the master configuration. Note that if a MAC interface communicates with only one PHY, a feature like polling is not necessary because the MAC always communicates with the same PHY address. This feature delays the master configuration as the MAC has to constantly read the alive status of each PHY address.