DUT and LP need to be on an insulating surface, 10cm above earth ground
The CDN needs to have 0.1 - 0.3m separation to the DUT and LP
Cable needs to be 30-50mm above earth ground
CDN needs to match corresponding cable types
Attenuator between the test equipment and CDN
Verify the cable before the attenuator does not have any contact with the system such as DUT, LP, Ethernet cable, cable after attenuator. This can result in high amplitude noise direct injected into the system without attenuation
Figure 4-11 CI Test Setup
Note:
Further details on the CI test setup and waveform and test setup can be
found in the IEC 41000 4-6 standard.
Capacitive clamping is also allow for CI testing if CDN is not
available.