SNLU223D August 2017 – February 2023 DS90UB954-Q1
If the following window opens after starting the ALP software, double check the hardware setup.
It may also be that the USB2ANY driver is not installed. Check the device manager. There should be a “HID-compliant device” under the “Human Interface Devices” as shown in #SNLU2239371.
The software should start with only “DS90UB954” in the “Devices” pull down menu. If there are more devices then the software is most likely in demo mode. When the ALP is operating in demo mode there is a “(Demo Mode)” indication in the lower left of the application status bar as shown in #SNLU2237984.
Disable the demo mode by selecting the “Preferences” pull down menu and un-checking “Enable Demo Mode”.
After demo mode is disabled, the ALP software will poll the ALP hardware. The ALP software will update and have only “DS90UB954” under the “Devices” pull down menu.