SNLU226B February 2018 – April 2021 DS90UB960-Q1
If ALP opens with the incorrect profile loaded the correct profile can be loaded from the USB2ANY/Aardvark Setup found under the tools menu.
Highlight the incorrect profile in the Defined ALP Devices list and press the remove button.
Find the correct profile under the Select a Daughter Board list, highlight the profile and press Add. If DS90UB960 ALP profile is not listed, contact your TI representative to obtain it. The ALP profiles are typically located in the ALP installation directory such as "C:\Program Files (x86)\Texas Instruments\Analog LaunchPAD v1.56.0010\Profiles\".
Select Ok and the correct profile must now be loaded.