SNLU262A december 2019 – june 2023 DP83826I
The on-board MSP430 comes pre-programmed and ready to use. When using this EVM for the first time on a Windows 7 (or above) PC, MSP430 drivers and USB-2-MDIO software utility will have to be installed. USB-2-MDIO software can be used for accessing the PHY's registers. In the case where an external MSP430 or EZFET is needed, the user may simply connect the TST and RST pins of their device to the DP83826EVM.