SNLU341A December 2023 – July 2024 MCT8314Z
The MCT8314ZEVM includes a MSP430FR2355 low-power MCU to provide the pulse-width modulation (PWM) signal required to commutate the motor. The MCU outputs a 20kHz PWM signal (PWM_MSP). The duty cycle (ranging from 0–100%) of the PWM output by the MCU is controlled by the potentiometer R6. The motor speed increases the more the potentiometer is turned counterclockwise, and decreases when turned clockwise. To select whether the PWM signal from the MSP or an external PWM is sourced to the MCT8314Z, use the PWM_SEL jumper J1.
To program the MSP430FR2355, an external MSP430 FET programmer must be connected to the Spy-Bi-Wire (SBW) interface connector J4. Many MSP430 LaunchPads™ provide an on board eZ-FET Debug Probe that can be jumper-wired to the MCT8314ZEVM to flash the firmware into the MSP430FR2355 microcontroller.
The Reset (RST) button at any time to restart the MCU program. Two active-low LEDs, D4 and D5, can be used for debug purposes as well.
The 18-pin shunt jumper bridge J6 ties all signals between the microcontroller and the MCT8314Z device. These jumpers can be inserted or removed as needed to isolate the microcontroller from the gate driver. This allows for microcontroller signal debugging or using the MCT8314ZEVM as a standalone gate driver with an external microcontroller.