Download the latest version of Code Composer
Studio. This sets up a folder at the directory C:\ti.
Accept all agreements, default
install locations, and select Next to proceed through menus.
In the Select Components
window, make sure to check MSP430 Low-Power MCUs to install the required
packages for the MSP430 LaunchPad Evaluation Kits.
After installing, run CCS and select a
folder or the default to use as the workspace to store any new projects. The location and
naming convention can be changed based on the user's preference. Click the OK button to
accept.
In CCS, click on the Project tab and
select Import CCS Projects. Click on Browse.
Select the folder created in step 1 by
extracting the MCT8314Z firmware.
Import the project into the workspace as
shown in Figure 4-3.
Figure 3-3 MSP430FR2355 Interface Firmware Code
in Code Composer Studio