SNOAA47A September 2024 – October 2024 TMP116 , TMP117 , TMP119
If the DUT temperature change is known as the corresponding dissipated power changes, there is the possibility to calculate the thermal resistance (RT) between the sensor and the thermal head.
This parameter is calculated as:
where
Estimating the 95% of step final temperature as a 3×τ point, it is possible to estimate the system time constant. Despite this self-heating and cooling process not fully matching the ideal Gaussian curve, the time constant remains a convenient way to estimate the process speed. Knowing the time constant and thermal resistance (RT), there is the possibility to calculate the sensor's effective thermal mass for each soldering case as:
There is importance in understanding that Equation 3 calculates the effective thermal mass, which is larger than the package thermal mass, because thermal mass also includes the connected PCB area around the soldered device.