The
H-bridge voltage supply (VH-Bridge) should be
at least:
In the previous circuit
shown, a 5-V supply is used for the H-bridge to give 0.5V of headroom
and accommodate for all of the voltage drops.
The H-bridge supply may
need to be increased if:
A higher voltage
is needed for the TEC.
FETs cannot be
turned ON fully and produce significant voltages drops.
Bidirectional current-sense
amplifier (U1A):
The current-sense
amplifier senses the current through the TEC using a sense resistor
(RSense). The output is used as feedback to the control
amplifier (U1C) which determines the gate drive strength (TEC
current).
RSense
selection:
Smaller values of
RSense give better power dissipation performance
and produce a lower voltage drop. Depending on the desired
system accuracy, small values require a precision amplifier with
great DC performance to accurately read the sense resistor
voltage.
RSense
for this circuit was chosen to be 50mΩ. A 50-mΩ resister
produces a voltage drop of 125mV at 2.5A. The LMP7704-SP has a typical offset
voltage of ±37µV which produces an error of about 0.75mA at peak
current.
U1A Gain
Selection:
The current-sense
amplifier gain is determined by the resistors R1, R2, R3, and
R4
In the previous
circuit shown, it is desirable to measure the current as a
voltage level by adjusting U1A gain. The chosen gain for the
current-sense amplifier is G = 20.
A TEC
current of 2.5A equates to a 125mV across
RSense. 125mV across RSense
translates to 2.5V (125mV × 20) at the output of U1A.
The gain selection produces a 1-to-1 relationship
between the current through the TEC and the output
voltage of the current-sense amplifier.
Gain selection
equations:
Following the
previous equations always results in a 1-to-1 relationship
between the TEC current and the output voltage of the
current-sense amplifier.
Voltage Reference Selection (U1B):
A single-supply
op amp is not able to measure current bidirectionally unless it
has a DC offset. If no offset is used, the output of the
amplifier saturates when the current has the opposite sign of
the voltage supply of the op amp. This is why a voltage
reference is used to generate a DC offset and prevent
saturation.
Reference voltage
value selection:
The
voltage reference needs to be at least equivalent to the
expected maximum current through the TEC. If 2.5A is the
rated Imax of the TEC, then at least a 2.5-V
reference must be used to account for the current range
of –2.5A to 2.5A. It is also paramount to account for
the output swing limitation (VO) of the
amplifier.
A
reference voltage of 2.75V was chosen due to the
amplifier negative output rail limitation of (V–) +
0.2V.
The voltage divider formed by R5 and R6 is fed to
one of the LMP7704-SP channels (U1B)
as a buffer. The voltage divider generates the
reference voltage of 2.75V.
To adjust the output of the reference, use the
following equation:
The accuracy of the voltage reference depends on
the tolerance of the resistors in the
divider.
With a voltage reference, calculate the output
voltage of the current-sense amplifier as
follows:
As the current through the TEC goes from –2.5A to
2.5A, the output voltage of the current-sense
amplifier goes from 0.25V to 5.25V (2.75V is
equivalent to 0A).
If the negative rail output swing limitation of
the chosen amplifier is not accounted for, the
current-sense amplifier could saturate and cause
the rest of the system to saturate to the maximum
possible negative current. The value of the
saturated current through the TEC could be more
than 2.5A and it would depend on the H-bridge
supply voltage and gate drive capability.
Fortunately, the LMP7704-SP is a
rail-to-rail output amplifier so 0.25V is
satisfactory to mitigate the output swing
limitation. A different amplifier with less swing
requires more headroom from the voltage
reference.
Voltage Supply
Selection:
The voltage
supply of the current-sense amplifier must be above the maximum
expected output Vmax and the maximum output swing
limitation VO.
The chosen
amplifier supply is 10V which meets these requirements.
Failing to
consider the positive output swing limitation can result in the
system saturating to the maximum positive TEC current. The
maximum positive TEC current could be more than 2.5A (similar to
the case of saturating to the negative supply mentioned in the
Voltage Reference Selection
section).
Control Amplifier (U1C):
The control amplifier U1C
controls the gate drive strength (discussed in Gate Drivers (U1C and U1D)). To determine the
gate drive strength and direction, it compares the output from the
current-sense amplifier to a control input. The control
input (VIN) can come from a PID or an averaged PWM (usually
as an output of a temperature control loop). Since an op amp drives its
output until both its input terminals are at the same voltage level,
VIN is what determines the desired current level through
the TEC.
To control the current
through the TEC, set the control input, VIN, to a voltage
from 0.25V to 5.25V. The control amplifier output goes as high or as low
as needed to reach the point where the feedback (U1A output) and
VIN are at the same level. Calculate the set TEC current
level according to the control input voltage (VIN) and the
voltage reference of the current-sense amplifier
(VREF):
A VIN of 0.25V
means the control amplifier changes its output until –2.5A is sensed
through the TEC. Similarly, a 5.25-V input signal means the control
amplifier changes its output until 2.5A is sensed through the TEC.
This behavior can
be susceptible to oscillations; therefore, components R1 and C1
are added to not allow for the output of the control amplifier
to change instantaneously. The values were chosen to induce at
least 60° of phase margin as shown in the AC Simulation Results section.
Gate Drivers (U1C and
U1D):
The gate drivers are
responsible for providing gate signals to each half-bridge.
Gate driver
functionality:
Taking a look at
either gate driver and its corresponding half-bridge:
When the
output of the gate driver is a high voltage this only
turns ON the N-channel FET (Q2 or Q4). When the output
is a low voltage, the P-channel FET is ON (Q1 or Q3).
It is important to consider if there is any point
where three FETs can be ON simultaneously. This is
discussed in the MOSFET Selection section.
An
isolation resistor (Riso) is added to prevent
instability when driving the FETs capacitive load. The
value of R8 and R16 is calculated with the following
equation:
To set the
maximum output voltage of the gate drivers
(VmaxDriver), change the reference voltage TL1431-SP (U2) applied to U1D.
Ensure that VmaxDriver is within the output
swing capability of the chosen amplifier. In this case
the LMP7704-SP output swing is 0.2V from
the positive rail; therefore, the maximum VmaxDriver
is 9.8V.
R13 is used to limit
supply current when biasing the cathode. Ensure
that R13 provides more than 1mA to
U2:
Setting
VmaxDriver Voltage:
In the
previous design shown, the maximum driver output voltage
is equivalent to double the reference voltage due to the
non-inverting gain being G = 2.
Note that
VmaxDriver is the maximum voltage the
gate driver U1D could ever produce. However,
VmaxDriver is not the maximum voltage
applied to the H-bridges by the gate drivers to
generate 2.5A through the TEC
(VmaxGate). VmaxGate
depends on the MOSFETs selected and
VH-Bridge. Determine VmaxGate
through simulation or by looking at the MOSFET data
sheets and identifying the VGS required to
attain Imax. Simulation showed that a maximum
VmaxGate of 8V (worst-case FET threshold
voltages) is needed to achieve 2.5A through the TEC.
Ensure that VmaxDriver is above the
maximum VmaxGate by the amount of
output swing limitation of the control amplifier
(VO(U1C)):
VmaxDriver needs to be above
VmaxGate to ensure that the control
amplifier (U1C) does not saturate into the
negative rail.
Inverting gate
driver signals:
It is important
to note that if both gate drivers (U1C and U1D) tracked each
other, then all 4 FETs will turn ON at the same time. This is
undesirable as it causes shoot-through current. The ideal
behavior is that only one of the two diagonal pairs of FETs is
turned ON. The diagonal pairs being (Q1 and Q4) OR (Q3 and
Q2).
To
achieve this behavior, the output of U1C is connected to
the inverting input of U1D. Looking at how this works:
U1D defaults its output to VmaxDriver.
However, as the minimum 0.25V VIN is applied,
the output of U1C will slightly increase and settle
until –2.5A is sensed. This causes the output of U1D to
be at VmaxGate. As VIN changes,
the relationship between both gate driver outputs is
defined as follows:
This
causes the outputs to linearly track each other and in
opposite directions, that is, when U1D is at 9V then U1C
is at 0V.
This is why VmaxDriver needs to be
above VmaxGate by VO(U1C):
to avoid a situation where the output of the U1C
is at 0V since it can only swing down to 0.2V of
the negative rail (GND).
Assuming that the MOSFET threshold voltages are
accounted for, this gate driver design ensures
that only one of the two aforementioned diagonal
pairs is ON during operation.
Amplifier
selection:
Ensure that the
op amp chosen has enough output swing to support the desired
maximum voltage. The LMP7704-SP can swing to 0.2V of the
positive supply (9.8V).
MOSFET Selection:
The FET threshold voltage
is critical to obtaining a working design. During operation, only one
pair of the diagonal FETs must be turned ON at a time. The pairs being:
(Q1 and Q4) or (Q3 and Q2). If three FETs were to be ON simultaneously,
for example – Q1, Q2, and Q4 then the H-bridge supply rail could connect
to GND with a very small resistance through Q2 and cause a spike in
current known as shoot-through current. This could damage the FET and
lead to system failure. To avoid this, it is absolutely crucial to have
only one of the diagonal FET pairs turned ON at a time.
For the circuit
shown, the FETs selected all have a minimum threshold voltage
(Vth) of 2V (N-channel) or –2V (P-channel).
This
means a 2.5-V gate signal, without the resistor divider
on the N-channel FETs, can turn ON both the high-side
and low-side FET of the same half-bridge and cause
shoot-through current.
To ensure this does not happen, a voltage divider
is added for the N-channel FETs. Choose the
voltage divider such that when the P-channel FET
is about to turn ON, the N-channel FET, driven by
the same gate signal, should be off. For the
chosen FETs that have a Vth of 2V, it
was chosen that the N-channel FET gate
(VN-Gate) should be at 1.9V
when 3V is an output of a gate driver. Calculate
the voltage divider as follows (assume
RTOP = 100kΩ and ensure that
VN-Gate is lower than the minimum
N-channel Vth):
With the
previously-calculated resistor divider, if a 2.5-V gate signal
is applied to turn ON the P-channel FET then the N-channel gate
only sees 1.6V and therefore it is off. This ensures only one of
the diagonal pairs of FETs is ON during operation.
Ensure
that the gate can be driven high enough such that the
maximum Vth of the FETs (from the data sheet)
can still be used with the resistor divider. According
to the data sheet, the maximum Vth is 4V.
When an absolute maximum VmaxGate (8.8V)
signal is applied, the maximum VN-Gate with
the divider is 5.56V. Ensuring turn ON at Vth
variation.
The absolute maximum VmaxGate without
saturating U1C is 8.8V and is derived based on the
following equation: