SNOAA76 August 2021 LDC3114 , LDC3114-Q1
To present a wide range of sensor resonant frequencies, an additional sensor that was used to prototype with the LDC3114EVM was Sensor R. The inductance of this sensor is a midpoint between the EVM sensor and Sensor N, at 1.026 μH with no target present. Sensor R has the following physical properties:
Figure 4-3 shows the raw data and frequency response of Sensor R. After the target reaches 20% of the sensor diameter, 0.8 mm, the frequency response begins to level off.