The LMG342XEVM-04X card can be modified to operate in bootstrap mode, where the 12-V bias voltage is used to power both LMG342XR0X0 devices. This mode can be achieved by the following modifications to the EVM:
- Remove R1.
- Place a 2-Ω resistor on R2.
- Place a 600-V SOD-123 diode on D1, such as UFM15PL-TP.
- Adjust Rdrv resistor for the low side to be above 70 kΩ, which corresponds to a slew rate below 60 V/ns for the low side. During starup, FAULT signal from the top GaN device is used to control Q1 on the bottom GaN device to operate it at lower slew rate. Once the bootstrap power supply is ready, the bottom GaN, U2 switch to normal operation which is higher slew rate.