SNVS871M July 2012 – June 2020
PRODUCTION DATA.
The LP8556 boost converter switching frequency can be set either by an external resistor (BOOST_FSET_EN = 1 selection), RFSET, or by pre-configuring EPROM memory with the choice of boost frequency (BOOST_FREQ field). Table 1 summarizes setting of the switching frequency. Note that the RFSET is shared for setting the PWM dimming frequency in addition to setting the boost switching frequency. Setting the boost switching frequency and PWM dimming frequency using an external resistor is separately shown in Table 5.