• Menu
  • Product
  • Email
  • PDF
  • Order now
  • LP87524B/J/P-Q1 Technical Reference Manual

    • SNVU663A June   2019  – May 2021 LP87524-Q1 , LP87524B-Q1 , LP87524J-Q1 , LP87524P-Q1

       

  • CONTENTS
  • SEARCH
  • LP87524B/J/P-Q1 Technical Reference Manual
  1.   Trademarks
  2. 1Introduction
  3. 2Setup
    1. 2.1 SCL/SDA Pins
    2. 2.2 NRST Pin
    3. 2.3 ENx (GPIOx) Pins
    4. 2.4 nINT
  4. 3Configuration
    1. 3.1 Default OTP Configurations
      1. 3.1.1 LP87524B-Q1 OTP Configuration
        1. 3.1.1.1 Startup and Shutdown Sequence
      2. 3.1.2 LP87524J-Q1 OTP Configuration
        1. 3.1.2.1 Startup and Shutdown Sequence
      3. 3.1.3 LP87524P-Q1 OTP Configuration
        1. 3.1.3.1 Startup and Shutdown Sequence
  5. 4References
  6. 5Revision History
  7. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

TECHNICAL REFERENCE

LP87524B/J/P-Q1 Technical Reference Manual

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

The LP87524B/J/P-Q1 contains four step-down DC/DC converter cores, which are configured as 4 single phase outputs. These devices power AWR1642 and AWR1243 automotive radar devices and IWR1642 industrial radar devices.

This technical reference manual can be used as a reference for the LP87524B/J/P-Q1 default register bits after OTP memory download. This technical reference manual does not provide information about the electrical characteristics, external components, package, or the functionality of the device. For this information and the full register map, refer to the LP87524B/J/P-Q1 Four 4-MHz Buck Converters for AWR and IWR MMICs datasheet.

2 Setup

There are a few important connections to ensure the LP87524B/J/P-Q1 is configured correctly, each of which are described in this section. Good examples of how to connect the radar devices to the LP87524B/J/P-Q1 PMICs are shown in Figure 2-1, Figure 2-2 and Figure 2-3. LDOs are not required as the device meets noise and ripple specifications with LC filters. Refer to XWR1xxx Power Management Optimizations – Low Cost LC Filter Solution application report.

GUID-20210519-CA0I-ZFJZ-2K8T-TB9ZZZWZWKTP-low.svg Figure 2-1 Typical Connection to LP87524B-Q1
GUID-5FDB3BBA-0039-4F31-A991-A23805E08F86-low.gif Figure 2-2 Typical Connection to LP87524J-Q1
GUID-089D1D10-0EAB-46FE-A746-3323D4CAECCD-low.gif Figure 2-3 Typical Connection to LP87524P-Q1

2.1 SCL/SDA Pins

The SCL and SDA lines (pins 5 & 6, respectively) are used to communicate between the MCU and the LP87524B/J/P-Q1 PMIC using an I2C compatible Interface. The I2C compatible synchronous serial interface provides access to the programmable functions and registers on the device. This protocol uses a two-wire interface for bidirectional communications between the IC's connected to the bus. The two interface lines are the serial data line (SDA), and the serial clock line (SCL). Every device on the bus is assigned a unique address and acts as either a master or a slave depending on whether it generates or receives the serial clock SCL. The SCL and SDA lines must each have a pullup resistor placed on the line and remain HIGH even when the bus is idle. The LP87524B/J/P-Q1 supports standard mode (100 kHz), fast mode (400 kHz), fast mode plus (1 MHz), and high-speed mode (3.4 MHz). For all I2C protocol details refer to the device datasheet.

2.2 NRST Pin

The NRST pin (pin 20) is used to reset the device logic/enable device internal logic and IO interface. When the NRST voltage is below threshold level all power switches, references, controls, and bias circuitry of the LP87524B/J/P-Q1 device are turned off. When NRST is set to high level (and VANA is above UVLO level) this initiates power-on-reset (POR), OTP reading and enables the system I/O interface. The I2C host must allow at least 1.2 ms before writing or reading data to the LP87524B/J/P-Q1. Device enters STANDBY-mode after internal startup sequence. The host can change the default register setting by I2C if needed. The regulator(s) can be enabled/disabled by ENx pin(s) or by I2C interface.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale