SNVU767A March 2022 – January 2024
This section describes the test points and connectors on the EVM and how to properly connect, set up, and use the LM63635DNEVM. Either the banana jacks on the top of the board or the card edge connector can be used for connections. See Figure 1-1 for the top of board connections and Figure 1-2 for the card edge connections. See the LM636x5-Q1 3.5-V to 36-V, 1.5-A, and 2.5-A Automotive Step-down Voltage Converter Data Sheet for details. The following lists the functions of the connections: