The LP5891Q1EVM can be powered either by the
TMS320F280039C LaunchPad with the USB power (when the current consumption is low) or
an external power supply (the LP5891Q1EVM and the TMS320F280039C LaunchPad are
powered separately). Single LP5891Q1EVM can be quickly set up and tested by
following these steps:
- USB Power supply from the
TMS320F280039C LaunchPad
- Download the code to the
TMS320F280039C LaunchPad with TI Code Composer Studio software.
- Put the J6 jumper on
"MCU5V" and the middle, and set the switch S1 towards "SOUTHOST" , which
are marked with red boxes in Figure 3-3.
- Connect BoosterPack
connectors (J1, J2) on the LP5891Q1EVM with the TMS320F280039C
LaunchPad, the connection method is shown in Figure 3-3.
- Power the TMS320F280039C
LaunchPad through the USB cable.
- External Power supply
- Download the code to the
TMS320F280039C LaunchPad with TI Code Composer Studio software.
- Put the J5 jumper on
TP1 5V and EX 5V. Then put the J6 jumper on
EX5V and the middle. Set the switch S1 towards
SOUTHOST.
- Connect BoosterPack
connectors (J1, J2) on the LP5891Q1EVM with the TMS320F280039C
LaunchPad, the connection method is shown in Figure 3-3.
- Power the TMS320F280039C
LaunchPad through the USB cable.
- Connect TP1 and TP2 to
5V/GND power source.
- Power on 5V/GND power
supply.