SNVU868A September 2023 – April 2024
The LP5813/LP5812EVM can be converted for testing the LP5811/LP5810, which are from the same device family, by removing the factory-installed device (U1/U2) and replacing with the LP5811/LP5810 counterpart. When testing the LP5811 device, select the direct mode jumper setting and corresponding tag from the menu on the GUI start page to start evaluation.
This user’s guide describes the characteristics, setup, and usage of the LP5813/LP5812 evaluation module (EVM). The LP5813/LP5812EVM helps the user evaluate the features of the Texas Instruments LP5813 synchronous boost 4 × 3 matrix RGB LED driver and LP5812 4 × 3 matrix RGB LED driver, which integrate autonomous control.
This document covers following topics: